EEPROM Values

The General Purpose ±28 V Gate Drive Modules have additional EEPROM values due to their configuration as either Common-Path or Split-Path.

If a Low-Side Gate Drive module is configured as Split-Path, there are additional fields in the Hardware Configuration > Calibration screen. These two fields are: Customer Nominal Off Resistance and Customer Actual Off Resistance.

 

After installing custom gate resistors on the modules, the modules must be calibrated before use. Calibration measures the resistor value and stores it in the module’s EEPROM.